Part Number: TXB0108
Hi....
Section 8.3.2 in TXB0108 datasheet mentioned about I/O drive strength of driver to TXB0108 should be +/-2mA.
Which device satisfy this condition as to get 2mA drive strength source should need swing of 8V approx. if TXB0108 is biased at 1.8V?
According to equation, Vt = Vcci/2 = 1.8V/2 = 0.9V. If we approximate this number to Vt = 1V, value come out will be 1V/4K = 0.25mA
Kindly clarify why 2mA source is needed? and if needed how equation is justifying this condition?
My customer wants to use this device for 1.8V to 3.3V conversion.
Mitesh