This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0102: TXS0102 is suitable for UART level shifter?

Part Number: TXS0102


Hi Sir,

Is TXS0102 the suitable solution for UART level shifter on 1.8V to 5V and the speed will be UART TX/RX max 3Mbps and UART is push pull?

Thank you