Part Number: LSF0102
Other Parts Discussed in Thread: LSF0108, , SN74AVC2T245, SN74AXC4T774
I'm currently using LSF0102 for my SPI interface to level shift the voltage from/to 3.3V to/from 1.8V. but the datasheet says it's only recommended for i2C and UART even when the speed of the level shifter can go up to 100MHz. For SPI, only LSF0108 is recommended. Why is it so? I have given a portion of LSF0102 datasheet below.