SN74LVC1G175-EP: Military Grade clarification

Part Number: SN74LVC1G175-EP
Other Parts Discussed in Thread: SN74LVC1G175

Hi Team,

Good day.

Datasheet of this device mentions that there is an available Military Grade option. However it is not clear which part number is the Military grade.

Could it be the V62/06633-01XE part?

Thanks to confirm.

Art

  • Hey Art,

    The datasheet actually states 'Available in Military Temperature Range' meaning that it can be operated in the -55 to 125C. That doesn't mean that it is MIL-PRF-38535 qualified if that's what you're looking for.
    If you're looking for D-flip flops with military ratings, we don't seem to have any one channel options like the SN74LVC1G175, but there are a good range of 2 channel options.

    Thanks,
    Rami