Hello,
I am ready to move my project off the DK board to a custom one. However, I am confused about programming the TIVA. I was going to bring out the JTAG pins on the custom board to a connector. These pins are unused on the end product. I assumed that any JTAG programmer would be usable to the program the "board" in a production environment but, Im finding it is not so cut and dry. Is there a stand alone programmer that can be used to program the TIVA chips? My thought was that I could purchase hardware that would plug into a PC on one end(USB) and into the JTAG connector on the other end and we could then transfer the executable code to the processor.
Thanks for the help