Part Number: EK-TM4C123GXL
Hi,
I have powered the EK throught the target USB, the burned application starts and work but the USB port of debugger is enumerated but doesn't works.
Any suggestion?
Best regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: EK-TM4C123GXL
Hi,
I have powered the EK throught the target USB, the burned application starts and work but the USB port of debugger is enumerated but doesn't works.
Any suggestion?
Best regards
I am able to power my EK_TM4C123GXL through the target USB connector (the connector on the side) with the power switch in the "Device" position (to the left). I have a second USB cable connected to the debug port (on the top). I am able to debug using Code Composer Studio and I am able to use the virtual serial port. Can you provide some more details so that I may attempt to duplicate your issue?
Hi Bob
Some more detail...
I have powered the EK not using the target USB connector but using a DC/DC converter connected to the VBUS pin of the header connector then I have put the switch in target position.
In this situation if I connect the USB (debug) to the PC and after I power the EK the VCOM enumerate and works correctly, in this situation if I unplug and plug again the USB sometimes the VCOM enumerate but communication is not active.
The application writes data packet at 10ms continously over the VCOM and I can see data on the Tx test point..
Best Regards
I suspect the issue is that the ICDI chip which creates the virtual serial port needs to be reset when the debug USB connector is unplugged and then re-plugged.
Is there a reason that you power the launchpad this way? Can you cycle power on the external VBUS supply before attaching the debug USB cable?
Hello Luca,
If I understand right about your use of VBUS then that would be a +5V signal. I would not power the LaunchPad from VBUS.
See this app note on how to connect Host Mode for the EK-TM4C123GXL: https://www.ti.com/lit/pdf/spna243
Best Regards,
Ralph