Part Number: TM4C129XNCZAD
Hello, I am trying to write to and read from W25Q128JV FLASH memory by Winbond. I have a simple code right now that is supposed to enable write operation and read back the value of status register 1, which has write enable status on bit-1. I am getting all 0s on the read even though the expected value is 0x02 for write enabled status. Any help would be appreciated since I am not sure if it is my write or read that is faulty.
Here is the code I have://Disable the SSI module to change the settings for Memory communication.
SSIDisable(SSI3_BASE);
//make sure the polarity and phase configuration is correct for Memory communication
SSIConfigSetExpClk(SSI3_BASE, ui32SysClock, SSI_FRF_MOTO_MODE_3, SSI_MODE_MASTER, 2000000 , 8);
//Enable the SSI module after settings change.
SSIEnable(SSI3_BASE);
GPIOPinWrite(PQ_SPI_PORT, PQ1_SPI_SS_MEMORY_PIN, 0x0);
//Send the data over SPI.
SSIDataPut(SSI3_BASE, 0x06 );
while(SSIBusy(SSI3_BASE)){
}
//Turn SS pin high to finish write enable.
GPIOPinWrite(PQ_SPI_PORT, PQ1_SPI_SS_MEMORY_PIN, PQ1_SPI_SS_MEMORY_PIN);
GPIOPinWrite(PQ_SPI_PORT, PQ1_SPI_SS_MEMORY_PIN, 0x0);
//Send the data over SPI.
SSIDataPut(SSI3_BASE, 0x05 );
SSIDataGet(SSI3_BASE, (uint32_t *) &Laser.Miscellaneous.Monitor.TECSupplyVoltage);
while(SSIBusy(SSI3_BASE)){
}
GPIOPinWrite(PQ_SPI_PORT, PQ1_SPI_SS_MEMORY_PIN, PQ1_SPI_SS_MEMORY_PIN);
Here is the SPI initialization code I have:
uint32_t ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_240), 50000000);
//enable the pins used for SPI communication.
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOQ)){
}
//
// Configure the SS pin and communication pins as GPIO output pins.
//
GPIOPinTypeGPIOOutput(PQ_SPI_PORT, (PQ3_SPI_RX_PIN |
PQ1_SPI_SS_MEMORY_PIN |
PQ4_SPI_SS_DIGIPOT_PIN |
PQ5_SPI_SS_DAC_PIN));
//drive the clear pin high.
GPIOPinWrite(PQ_SPI_PORT, PQ3_SPI_RX_PIN, PQ3_SPI_RX_PIN);
//
// Enable the SSI3 peripheral
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI3);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_SSI3)){
}
GPIOPinConfigure(GPIO_PQ0_SSI3CLK);
GPIOPinConfigure(GPIO_PQ2_SSI3XDAT0);
GPIOPinTypeSSI(PQ_SPI_PORT, ( PQ0_SPI_CLK_PIN |
PQ2_SPI_TX_PIN ));
//
// Configure the SSI.
//
SSIConfigSetExpClk(SSI3_BASE, ui32SysClock, SSI_FRF_MOTO_MODE_3, SSI_MODE_MASTER, 2000000 , 12);
//
//Enable the SSI module
//
SSIEnable(SSI3_BASE);
//Set the SS pins to high to disable communication.
GPIOPinWrite(PQ_SPI_PORT, PQ1_SPI_SS_MEMORY_PIN, PQ1_SPI_SS_MEMORY_PIN);
GPIOPinWrite(PQ_SPI_PORT, PQ4_SPI_SS_DIGIPOT_PIN, PQ4_SPI_SS_DIGIPOT_PIN);
GPIOPinWrite(PQ_SPI_PORT, PQ5_SPI_SS_DAC_PIN, PQ5_SPI_SS_DAC_PIN);
SSIIntEnable(SSI3_BASE, SSI_TXFF);
Here is the write enable and read status register 1 instructions from the datasheet:


As far as I understand this device should work with either mode 0 or mode 3 SPI communication and I have tried both.