This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1231D5PM: [ERROR] CORTEX_M4_0: Error connecting to the target

Part Number: TM4C1231D5PM
Other Parts Discussed in Thread: UNIFLASH, CC1350

Hello,

I have build new board with TM4C1231 micro-controller. Controller basic schematic i have copied from  TM4C1231  launchpad. Right now I am using EK-TM4C1294XL board for programming but I am facing [ERROR] CORTEX_M4_0: Error connecting to the target. I have checked Controller VDD(3.3V), VDDC (1.2V) also remove cap from RST pin ( Only pull up on RST pin). I have upgraded  EK-TM4C1294XLEK-TM4C1294XL ICDI firmware from LM flash tool but fail to unlock procedure. 

Please help to program device