This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS0714: Unable to halt device

Part Number: TMS570LS0714


Hello, everyone. Recently, when I used tms570ls0714 chip with spi-dma function, the chip could not be debugged due to the wrong configuration.

The test connection is successful, but an error will be reported when debugging the burning program as following : error connecting to the target: error - 2062 @ 0x0 unable to halt device. It seems that the address  of the buf register of SPI was incorrectly written during DMA configuration. What methods can I use to re-debug the chip or erase the internal programs of the chip?

What's more, it seems that I could not configure the boot pattern as C2000 chip, so that I cannot start my program from the RAM.Thanks.

Best Regards,

LiHua