This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM44L520: ESM -> Stat3 error (When downloading basic Halcogen source to RM44L520)

Part Number: RM44L520
Other Parts Discussed in Thread: HALCOGEN, TMS570LS1224, SEGGER

hello. I was only using the TMS570LS1224 EVM, and after learning some basic usage, I chose a TI MCU (RM44L520) to apply to my first project and downloaded the source code generated by HALCoGen to the MCU for debugging.

I used the latest version of CCS and the latest compiler, and also used the generated sys_link.cmd without modification.

I put a simple code for confirmation only in the main function below.

As a result, in the _c_int00() function, the value of esmREG->SR1[2] becomes 0x80 as shown below.

After searching datasheet Tables 6-31 and 6-32, it was confirmed that FMC uncorrectable error - Bus1 and Bus2 accesses (does not include address parity error) occurred.

The debugger uses XDS200/Segger J-link and the editor uses CCS/IAR, but they are the same.

I referred to the answers on the forum, but it didn't solve the problem.
Since I am a beginner, I would appreciate it if you could easily tell me step by step which part needs to be modified/supplemented.

1. CCS linker menu options

2. sys_link.cmd settings

3. etc...