This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570: DMA & SCI Multi-Buffer Mode

I am attempting to configure a DMA channel to fill the TMS570's SCI1 Tx multi-buffer (i.e., TD[0..7]) with 8 characters.  According to the "TMS570LS Series Technical Reference Manual" (SPNU489B, January 2011) section 13.6.2.2 and section 13.14.28, a Tx operation will be initiated in multi-buffer mode when a value is written to TD[0] (address 0xFFF7_E474).  This would suggest that I would want to program the DMA to write to TD[7..1] first, followed lastly by a write to TD[0].  That is, I'd want the DMA to write to the following sequence of destination addresses: 0xFFF7_E47B, E47A, E479, E478, E477, E476, E475, followed lastly by 0xFFF7_E474 which would trigger the Tx operation. However, I don't see any way to program the DMA to generate this sequence of addresses since it appears that all DMA addressing modes will only increment the destination address rather than decrement.  Are the EIDX/FIDX values signed?

Thanks.