Part Number: LP-MSPM0C1104
Tool/software:
Hi, experts:
I used CCS Theia 1.3.1 to set PWM configuration of 20 WQFN in LP-MSPM0C1104, I set TIMA0 as PWM source and enable all 4 channels, the PWM Period Count is set to 1000, when I use
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LP-MSPM0C1104
Tool/software:
Hi, experts:
I used CCS Theia 1.3.1 to set PWM configuration of 20 WQFN in LP-MSPM0C1104, I set TIMA0 as PWM source and enable all 4 channels, the PWM Period Count is set to 1000, when I use
Hi Bill,
What the pwm mode you are using? Edge-ailgn mode or central-align mode.
Maybe you could implement force output low to finish the function:
https://www.ti.com/lit/an/slaaek4/slaaek4.pdf

B.R.
Sal
Hi,Sal:
I found if pass 999(1000 - 1) to DL_TimerA_setCaptureCompareValue, PWM output will be low level, can you confirm it is the correct way?
Bill
Hi Bill,
I want to note that, if you set the pwm period as 1000, it will automatically set (1000-1) into load register to set the pwm period. So it should be correct to keep high or low (this depends on your pwm configuration) if you give CC value as 999.
B,R,
Sal