This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2431: There is something unclear about TRM "1.5.4.8.1.3.3.1 Receive (RX)"

Part Number: AM2431

Tool/software:

The TRM refers to spruim2g.pdf.

TRM "1.5.4.8.1.3.3.1 Receive (RX)" states, "However, received XON1/XOFF1 characters must be written to the RX FIFO if the subsequent character is not XON2/XOFF2."
The above sentence says "must be written," so does this mean that it needs to be written on the software side?
It also says that it needs to be written, so I would like to know how to do this.

Thank you in advance for your help.

  • Hello 

    Thank you for the query and your inputs to improve the SOC collaterals.

    I see the following threads assigned to me and i suspect you may have additional queries (threads) that may be answered by other members supporting customers.

    Could you please consolidate all the queries into a single thread on a day basis ( i see the difference between thread are a few minutes) or at the least 5..6 queries into a single thread or queries related to a specific section or chapter in the TRM into a single thread, it would be easy for us to track and reply.

    More threads could possibly result in delayed response or missed response compared to providing response for consolidated threads.

    I will close this thread. Please start a new thread (consolidate multiple threads into a single thread) to provide focused support.

    Please expect delay in response since as i will have to check internally with multiple teams to get the queries answered.

    Regards,

    Sreenivasa