Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi TI-Experts,
I am struggeling with the Baud Rate Config.
I am using normal CAN, not CAN FD.
But I don't know what is the relevance of
1a. the "arbitration baud rate" and
1b. the "data baud rate"?
2. Does the "data baud rate" only apply to CAN FD or is it also relevant for normal CAN?
3. Should I enter something for "desired data rate"?
4. What is the relationship between the CAN CLK frequency, the arbitration and the data baud rate and the corresponding bit timing parameters?
5. I have noticed that with a CAN clock frequency of 80 MHz I do not receive some CAN messages and then the MRAF bit is set in the interrupt register. However, if I reduce the CAN clock frequency to 40 MHz, I achieve very reliable CAN message reception - apparently without MRAF errors. The sysconfig does not give an error when I set the 80 MHz, but is it perhaps still the case that the CAN module cannot process a CAN clock frequency of 80 MHz and can only cope with a maximum of 40 MHz, for example? I didn't find any corresponding information in the TRM.
Thanks a lot for your answers in advance!
Matze