Tool/software:
Hi team,
I would like to confirm the following IOMUX init digital output library.
It is stated that the "GPIO functionality is always a pin function of 0x00000001, but i do not understand what that means.
As i checked on the TRM for IOMUX register, i think it the setting for Peripheral function but i do not know why it should be set as 0x00000001.
Could you please help me to understand ?

__STATIC_INLINE void DL_GPIO_initDigitalOutput(uint32_t pincmIndex)
{
/* GPIO functionality is always a pin function of 0x00000001 */
IOMUX->SECCFG.PINCM[pincmIndex] =
(IOMUX_PINCM_PC_CONNECTED | ((uint32_t) 0x00000001));
}
Best regards,
Kenley