This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: AM243x-LP Failing module initialization

Part Number: AM2434

Tool/software:

Hi there,

I am having some problems with this function: 
int32_t SOC_moduleClockEnable(uint32_t moduleId, uint32_t enable);

After soc initialization, I can download gpio example program toggling an LED. It works. This is our own prototype board.

However, I then download an application that has more modules. 
int32_t SOC_moduleClockEnable(uint32_t moduleId, uint32_t enable); fails for each module, I worked around the assert by changing the return value in debug mode in CCS to iterate all modules.

Here are my modules:

uint32_t gSocModules[] = {
TISCI_DEV_FSS0,
TISCI_DEV_FSS0_FSAS_0,
TISCI_DEV_FSS0_OSPI_0,

TISCI_DEV_PRU_ICSSG1,

TISCI_DEV_UART2,

SOC_MODULES_END,
};


how to debug the problem?

Best regards,
Jinlong