This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2432: CRC error and frame time outs

Part Number: AM2432

Hi TI experts,

 

One month ago I asked about this,

AM2432: Drive returns malformed packets with Innovance H5U PLC after reconnect the drive. EtherCAT - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

With the changes suggested: #define ENABLE_MULTIPLE_SM_ACCESS_IN_SINGLE_DATAGRAM     1

We found that our product may generate more crc errors and frame time outs.

We are using Omron PLC with 26 drives, 23 of them are AM2432 and the rest are XMC 4800. When ENABLE_MULTIPLE_SM_ACCESS_IN_SINGLE_DATAGRAM is 0. CRC errors is 0 for 12 hours.

frame timeouts.png

CRC errors is also 0.

crc errors.png

When ENABLE_MULTIPLE_SM_ACCESS_IN_SINGLE_DATAGRAM is 1, and test time is only 3 hours,

The frame time outs is 33 for 3 hours,

withH5U_frame_timeout.jpg

The maximum CRC error is 42

5f2bea35-54d0-472e-aabe-a93646aabed9.jpg