This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Documentation bug for DMAPCR PARITY_ENA

Hello,

I think there is a documentation bug in table 16-66 in the description of the PARITY_ENA field.  It says initially that 5h will disable the parity check (this is the default value, so I am guessing this is correct), and all other values will enable parity checking.  Then, there is a note that says "It is recommended to write a 5h to enable parity check, to guard against soft errors from flipping PARITY_ENA to a disabled state."  I am guessing that should read "to write an Ah to enable...".  Please correct me if I am incorrect.  Thanks.