Other Parts Discussed in Thread: RM48L952
What is the difference between these two parameters for the RM48L952?
- ICCREFHI (max. 3 mA) ADREFHI supply current
- IADREFHI (max. 10 mA) ADREFHI input current
At first glance, it looks like it should be either one or the other.
Reference
Datasheet RM48L952 16- and 32-Bit RISC Flash Microcontroller
Find, "ADREFHI input current"
Find, "ADREFHI supply current"