This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TivaWare ROM_TimerIntClear question

In the TIVA ROM datasheet for the ROM_TimerIntClear() method, it states:

"Because there is a write buffer in the Cortex-M processor, it may take several clock cycles before the interrupt source is actually cleared. Therefore, it is recommended that the interrupt source be cleared early in the interrupt handler (as opposed to the very last action) to avoid returning from the interrupt handler before the interrupt source is actually cleared. Failure to do so may result in the interrupt handler being immediately reentered (because the interrupt controller still sees the interrupt source asserted)."

If I call ROM_TimerIntClear() in my ISR, and the timer expires again.  Will the ISR be entered again while i'm still in the ISR, or will it wait until the ISR has completed before servicing the ISR again?

Thanks