This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Transmit a Broadcast ARP

Other Parts Discussed in Thread: HALCOGEN

Hello,

I cannot get the EMAC on an RM46x HDK to transmit a broadcast ARP request. I verified the packet is correctly formed and is sent to the hardware. The RM46x HDK can receive a broadcast  ARP and respond OK. The result of this is before I can transmit Ethernet traffic to a network node, I must "ping" the RM46x" from the node first so that the RM46x HDK ARP table is updated with the network node's hardware address. The only setting for broadcast I see in HALCoGen is for the receive broadcast - I have that enabled. Am I missing a configuration setting somewhere? I'm using FreeRTOS with generated code from HALCoGen.

Thank you for your help,

Ray