Hi All,
I have developed my board with TM4C123, I have flashed it using XDS100v2-ARM.
I can see that LED toggling code is working good.
When I tried to get clock it in debug mode it shows
SysCtlClockGet = 0x0000077C which is 1916 Hz, why it is too low ?
I dont have any external oscillator connected on board. I wanted to set something around 50 MHz.
SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ | SYSCTL_OSC_INT);
are these parameters correct ?