This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

error trying to connect XDS510 USB plus with RDK-IDM-L35 board.



Hi,

I would like a support to solve the error that I'm getting...

I'm using Windows 8.1 Single Language,

Code Composer Studio Version: 5.5.0.00077,

XDS510 USB PLUS

Stellaris RDK-IDM-L35 kit

The project makes well but when I try to debug I'm getting this error:

----------------------------------------------------------------------------------------------

Error connecting to the target: Error 0x80000240/-141
Fatal Error during: Initialization, OCS,
Error generated by SD scan controller module

----------------------------------------------------------------------------------------------

I have already tried the link for adapters connection

processors.wiki.ti.com/.../Stellaris_support_in_CCS

and

processors.wiki.ti.com/.../Creating_new_CCS_v5_Project_with_Stellarisware

but I am stopped at this error.

The project I am trying to debug is the "hello"

Please could some one help me?