Other Parts Discussed in Thread: BQ34Z100EVM
Hi,
I am using TMS570 launchpad (TMS570LS0432) to interface with BQ34Z100EVM (battery fuel gauge).
BQ34Z100EVM supports I2C protocol but TMS570LS0432 does not support I2C.
So, after searching on E2E community, I got to know that we can still communicate TMS570LS0432 and BQ34Z100EVM with N2HET.

I tried to run the program available in that example. But I could not figure out following points:
1. Which N2HET pins are used as SDA() and SCL() for I2C communication?
2. I am attaching the code snippet of main.c
/** @file sys_main.c
* @brief Application main file
* @date 9.Sep.2014
* @version 04.01.00
*
* This file contains an empty main function,
* which can be used for the application.
*/
/* (c) Texas Instruments 2009-2014, All rights reserved. */
/* USER CODE BEGIN (0) */
/* USER CODE END */
/* Include Files */
#include "sys_common.h"
/* USER CODE BEGIN (1) */
#include "het.h"
#include "HET_IO_TEST.h"
#include "HET_EMU.h"
unsigned char *I2C1_txptr = NULL, *I2C1_rxptr = NULL;
unsigned char I2C1_TxData[5] = {0, 0, 0, 0, 0};
unsigned char I2C1_RxData[20];
unsigned int Data_Send_HET = 0, Data_Rece_HET = 0;
unsigned int Data_Send_I2C = 0, Data_Rece_I2C = 0;
// unsigned int Stop_Rece_I2C = 0;
unsigned int Start_Repeat=0;
char IntEna =1;
char RW = 0; //write
char I2C_ADDR; // todo: jc 20141024 this is a hack to make the TI emukator code work, candidate for refactoring
char NumOfBytes = 1;
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
/* USER CODE END */
void main(void)
{
/* USER CODE BEGIN (3) */
// set the i2c address
I2C_ADDR = 0xAB;
int i;
NumOfBytes = 1;
char StopBit = 1;
volatile unsigned int wait_counter;
I2C1_txptr = I2C1_TxData;
I2C1_rxptr = I2C1_RxData;
hetInit();
hetREG1->INTENAS = 0xFFFFFFFFU; // todo jc 20141024 check if this is needed
hetREG1->GCR = 0x01010001; // todo jc 20141024 check if this is needed
_enable_IRQ(); // todo jc 20141024 check if this is needed
IntEna =1;
RW = 0; //write
NumOfBytes = 1;
I2C1_TxData[0] = 0x02; // % charge left
HetI2CPutAddr(I2C_ADDR, RW, NumOfBytes, IntEna, StopBit);
for(wait_counter=0;wait_counter<0x18;wait_counter++); //wait some time.
RW = 1; //Read
IntEna = 0;//no transmit interrupt
HetI2CPutAddr(I2C_ADDR, RW, NumOfBytes, IntEna, StopBit);
while(1);
/* USER CODE END */
}
/* USER CODE BEGIN (4) */
/* USER CODE END */
Please help me out to run the communication.
Thanks
Ritul Shah