Part Number: TMS570LS1227
Tool/software: Code Composer Studio
Team,
As a followup to the response to the following forum, e2e.ti.com/.../2370558
Could you please answer the following customer question.
-
i have a problem with the HET of the LC4357 Board.
This is my program
P02_Period PCNT { hr_lr=HIGH,type=RISE2RISE,pin=2};
;P02_HighTime PCNT { hr_lr=LOW,type=RISE2FALL,pin=2};
P02_EventCount ECNT { pin=2,event=RISE,reg=A,data=0};
P02_Branch BR { next=P02_Last,cond_addr=P02_PeriodSave ,pin=2,event=RISE};
P02_PeriodSave ADD { src1=REM,src2=ZERO,dest=IMM,remote=P02_Period,data=0};
P02_DJZ DJZ { next=P02_Add,cond_addr=P02_Move,reg=A,data=8}; Anzahl Nocken zu zählen
P02_Add ADD { src1=REM,src2=IMM,dest=IMM,next=P02_Last,remote=P02_Period,data=0};
P02_Move ADD { src1=REM,src2=ZERO,dest=IMM,remote=P02_Add,data=0};Ergebnis hier speichern
P02_ResetDJZ MOV32 { remote=P02_DJZ,type=IMTOREG&REM,reg=A,data=8};
P02_ResetSum MOV32 { remote=P02_Add,type=IMTOREG&REM,reg=A,data=0};
P02_Last BR { next=P00_Period,cond_addr=P00_Period,event=NOCOND};
P02_Period works fine, if I do not use (comment out) the P02_HighTime.
If I use the P02_Hightime there seems to be an Problem with the HR Data.
I don’t want to use HR Share, because I need the Pins.
For me it is ok, to have the P02_Hightime only with Low Resolution.
Where is my mistake
Thank you.
-Needhu