This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123GH6PGE: Question on USB endpoint usage when implementing multiple VCOM ports

Part Number: TM4C123GH6PGE

Hi all, when implementing a VCOM port, two endpoints are needed:

- One for control interface (In and Out)

- The other for Data interface (In and Out)

Does anyone know if the Control Interface can be shared when implementing multiple VCOM ports? In other words, the extra endpoints for the additional VCOM ports are needed for the data interface only? Or the control interface is per VCOM port therefore extra endpoints are required as the result?

I would appreciate any document or link on this regard.

Thank you!

Richard