This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL2-570LC43: TMAS570LC4357 LAUNCHPAD

Part Number: LAUNCHXL2-570LC43
Other Parts Discussed in Thread: HALCOGEN

Dear sir/Mam.

To  transmit data through UART(a frame of 10 bytes in interupt mode), Should i use LIN 1 module as SCI compatiblity mode or SCI3 module.I am trying to write code using scisend() in LIN1 module as SCI compatibility mode. But unable to do it. I need 1Mbps of baudrate(precise).I found precise 1 Mbps is possible in LIN1 module. Kindly help.I also need to receive data (a frame of 10 bytes)@1 Mbps.kindly help in configuration.

Thank you.