Part Number: TM4C123GH6PM
Iam using a TM4C123 series Launchpad and I wanted to use the ADC of the MCU in differential Mode.
I have gone through the Datasheet of the microcontroller But I could not understand the differential mode completely. Iam new to differential ADC's so would like clear my doubts
My Input signal is a 10 Hz sinewave (+/- 1V) or (2Vp-p) . Few of my questions are :
1.The ADC is unipolar differential Input or Bipolar differential Input?
2.VIN+ can have only positive input voltage or we can send negative voltage also? Will this pin read the negative cycle of the sinewave?
3.What voltage range should be given to VIN- Pin? Can we give it a constant voltage?
4.What is Input Common Mode voltage and what relation it has with the ADC Conversion?
5.If I amplify a low amplitude signal with an amplifier , What will be the maximum Gain I should set to be witihin the range of ADC? ( For Eg. Suppose the Original Signal is (+/- 1mv). How much Gain should I set?)