We uses 4MB of EXTERNAL-FLASH access over SPI bus.
I am looking for a way to easily program and burn data into the EXTERNAL-FLASH as part of manufacturing stage, and I have notice that LMFlash can access only internal FLASH and cannot access external FLASH (facilitating the SPI).
1. Is that so, or there is a “secret” way to use the LMFlash to access also external-flash somehow?
2. Is there is other tool that can burn external-flash (read/write) over same interface?
3. Any other recommended way to do so, without first burning program into internal-flash?
Thanks