Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: ENERGIA
Dear Experts,
now i am working with TivaC TM4C123GH6PM an energia. i never work in watch dog timer before so i was rewrite the watch dog timer example code(i get code from google) like below,
#include "driverlib/interrupt.h"
#include "driverlib/sysctl.h"
#include "driverlib/watchdog.h"
#include "driverlib/rom_map.h"
#include "driverlib/rom.h"
void setup()
{
Serial.begin(9600);
Serial.println("SETUP");
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_WDOG0); // Enable the watchdog peripheral
MAP_WatchdogReloadSet(WATCHDOG0_BASE, MAP_SysCtlClockGet() * 2); // Set timeout of watchdog to 2 sec
MAP_WatchdogResetEnable(WATCHDOG0_BASE); // Reset when watchdog expires
WatchdogIntRegister(WATCHDOG0_BASE, &WatchdogIntHandler); // Register the watchdog interrupt handler
MAP_WatchdogEnable(WATCHDOG0_BASE); // Enable the watchdog
if(SysCtlResetCauseGet() & SYSCTL_CAUSE_WDOG0) // Get and print the reset cause
{
Serial.println("Watchdog Reset");
}
else if(SysCtlResetCauseGet() & SYSCTL_CAUSE_EXT)
{
Serial.println("External reset");
}
SysCtlResetCauseClear(SYSCTL_CAUSE_WDOG0 | SYSCTL_CAUSE_EXT);
}
void loop()
{
Serial.println("MC Working");
delay(6000);
}
void WatchdogIntHandler(void)
{
WatchdogIntClear(WATCHDOG0_BASE); // Clear the watchdog interrupt.
Serial.println("REG CLEAR");
}
this code reset the watch dog timer register in every 2 sec, so watchdog is not resetting my controller, my doubt is this code is definitely reset the controller if my controller getting struck or hang for any disturbance.
please make sure about this.