Part Number: TMS570LS0432
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
I am using TI FEE example given by halcogen and its working, I am able to see only 8 bytes data getting printed .
and on every reset the data gets printed to the incremeted address.
Please refer the attached picture for reference.
could you please explain why only the same 8 bytes getting printed on every reset.
also, when I try to watch oResult=TI_Fee_Read(BlockNumber,BlockOffset,Read_Ptr,Length);
I always get 0 in oResult. I want to read the data written in that block. Please clarify the issue in detail.
Please help me, I just want to write some data and read them back.
my source code:
for(loop=0;loop<100;loop++)SpecialRamBlock[loop] = loop;
/* Initialize FEE. This will create Virtual sectors, initialize global variables etc.*/
TI_Fee_Init();
do
{
TI_Fee_MainFunction();
delay();
Status=TI_Fee_GetStatus(0 );
}
while(Status!= IDLE);
/* Write the block into EEP Asynchronously. Block size is configured in ti_fee_cfg.c file. Default Block size is
8 bytes */
BlockNumber=0x1;
TI_Fee_WriteAsync(BlockNumber, &SpecialRamBlock[0]);
do
{
TI_Fee_MainFunction();
delay();
Status=TI_Fee_GetStatus(0);
}
while(Status!=IDLE);
/* Write the block into EEP Synchronously. Write will not happen since data is same. */
TI_Fee_WriteSync(BlockNumber, &SpecialRamBlock[0]);
/* Read the block with unknown length */
BlockOffset = 0;
Length = 0xFFFF;
oResult=TI_Fee_Read(BlockNumber,BlockOffset,Read_Ptr,Length);
do
{
TI_Fee_MainFunction();
delay();
Status=TI_Fee_GetStatus(0);
}
while(Status!=IDLE);
while(1);