Part Number: TMS570LC4357
Hello,
We are using the TMS570LC4357 and we need more information about the PBIST ?
We perform the sequence below, otherwise, the writing of RINFOL and RINFOU is without effect and the PBIST is performed on all the regions (configuration by default):
- RINFOL and RINFOU registers are used to select the RAM groups.
- Then we have to clear the OVER0 bit in the OVER register (OVER0 is set to ‘1’ by default).
It seems to be different in the TMS570 reference manual and various explanation are given (see PBIST flow in section 9.3 or PBIST sequence section 9.1.3 where RAM group must be selected before OVER programming. But see also section 9.6.2 where OVER programming is performed before RAM group selection).
Could you tell us if this a documentation mistake and what is the good sequence to be performed ?
Best Regards,
Christopher