Other Parts Discussed in Thread: HALCOGEN
Hello,
We are trying to capture period and duty cycle for more than 8 signals. We are attempting to do this via a branch in the het1Program and change between two different signals we can look at. Is there a better way to try to go about it?
It seems like since I have the signals physically routed to the pins, I could also set up two edge counters as well and have one of these that we currently want as a capture to be configured as below - use the rising edge counter to calculate period and the both edges to calculate duty cycle? But do we then have to use the RTI to calculate the period? It seems like the het functions (besides capGetSignal) only give you a count of how many edges it sees, not the period of the signal.
Thanks!
hetINSTRUCTION_t het1PROGRAM[62U] =
{
/* CNT: Timebase
* - Instruction = 0
* - Next instruction = 1
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = na
* - Reg = T
*/
{
/* Program */
0x00002C80U,
/* Control */
0x01FFFFFFU,
/* Data */
0xFFFFFF80U,
/* Reserved */
0x00000000U
},
/* PWCNT: PWM 0 -> Duty Cycle
* - Instruction = 1
* - Next instruction = 2
* - Conditional next instruction = 2
* - Interrupt = 1
* - Pin = 31
*/
{
/* Program */
0x000055C0U,
/* Control */
(0x00004006U | (uint32)((uint32)31U << 8U) | (uint32)((uint32)2U << 3U)),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* DJZ: PWM 0 -> Period
* - Instruction = 2
* - Next instruction = 3
* - Conditional next instruction = 41
* - Interrupt = 2
* - Pin = na
*/
{
/* Program */
0x00007480U,
/* Control */
0x00052006U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PWCNT: PWM 1 -> Duty Cycle
* - Instruction = 3
* - Next instruction = 4
* - Conditional next instruction = 4
* - Interrupt = 3
* - Pin = 9
*/
{
/* Program */
0x000095C0U,
/* Control */
(0x00008006U | (uint32)((uint32)9U << 8U) | (uint32)((uint32)2U << 3U)),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* DJZ: PWM 1 -> Period
* - Instruction = 4
* - Next instruction = 5
* - Conditional next instruction = 43
* - Interrupt = 4
* - Pin = na
*/
{
/* Program */
0x0000B480U,
/* Control */
0x00056006U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PWCNT: PWM 2 -> Duty Cycle
* - Instruction = 5
* - Next instruction = 6
* - Conditional next instruction = 6
* - Interrupt = 5
* - Pin = 27
*/
{
/* Program */
0x0000D5C0U,
/* Control */
(0x0000C006U | (uint32)((uint32)27U << 8U) | (uint32)((uint32)2U << 3U)),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* DJZ: PWM 2 -> Period
* - Instruction = 6
* - Next instruction = 7
* - Conditional next instruction = 45
* - Interrupt = 6
* - Pin = na
*/
{
/* Program */
0x0000F480U,
/* Control */
0x0005A006U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PWCNT: PWM 3 -> Duty Cycle
* - Instruction = 7
* - Next instruction = 8
* - Conditional next instruction = 8
* - Interrupt = 7
* - Pin = 29
*/
{
/* Program */
0x000115C0U,
/* Control */
(0x00010006U | (uint32)((uint32)29U << 8U) | (uint32)((uint32)2U << 3U)),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* DJZ: PWM 3 -> Period
* - Instruction = 8
* - Next instruction = 9
* - Conditional next instruction = 47
* - Interrupt = 8
* - Pin = na
*/
{
/* Program */
0x00013480U,
/* Control */
0x0005E006U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PWCNT: PWM 4 -> Duty Cycle
* - Instruction = 9
* - Next instruction = 10
* - Conditional next instruction = 10
* - Interrupt = 9
* - Pin = 11
*/
{
/* Program */
0x000155C0U,
/* Control */
(0x00014006U | (uint32)((uint32)11U << 8U) | (uint32)((uint32)2U << 3U)),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* DJZ: PWM 4 -> Period
* - Instruction = 10
* - Next instruction = 11
* - Conditional next instruction = 49
* - Interrupt = 10
* - Pin = na
*/
{
/* Program */
0x00017480U,
/* Control */
0x00062006U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PWCNT: PWM 5 -> Duty Cycle
* - Instruction = 11
* - Next instruction = 12
* - Conditional next instruction = 12
* - Interrupt = 11
* - Pin = 21
*/
{
/* Program */
0x000195C0U,
/* Control */
(0x00018006U | (uint32)((uint32)21U << 8U) | (uint32)((uint32)0U << 3U)),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* DJZ: PWM 5 -> Period
* - Instruction = 12
* - Next instruction = 13
* - Conditional next instruction = 51
* - Interrupt = 12
* - Pin = na
*/
{
/* Program */
0x0001B480U,
/* Control */
0x00066006U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PWCNT: PWM 6 -> Duty Cycle
* - Instruction = 13
* - Next instruction = 14
* - Conditional next instruction = 14
* - Interrupt = 13
* - Pin = 4
*/
{
/* Program */
0x0001D5C0U,
/* Control */
(0x0001C006U | (uint32)((uint32)4U << 8U) | (uint32)((uint32)0U << 3U)),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* DJZ: PWM 6 -> Period
* - Instruction = 14
* - Next instruction = 15
* - Conditional next instruction = 53
* - Interrupt = 14
* - Pin = na
*/
{
/* Program */
0x0001F480U,
/* Control */
0x0006A006U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PWCNT: PWM 7 -> Duty Cycle
* - Instruction = 15
* - Next instruction = 16
* - Conditional next instruction = 16
* - Interrupt = 15
* - Pin = 31
*/
{
/* Program */
0x000215C0U,
/* Control */
(0x00020006U | (uint32)((uint32)31U << 8U) | (uint32)((uint32)0U << 3U)),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* DJZ: PWM 7 -> Period
* - Instruction = 16
* - Next instruction = 17
* - Conditional next instruction = 55
* - Interrupt = 16
* - Pin = na
*/
{
/* Program */
0x00023480U,
/* Control */
0x0006E006U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* ECNT: CCU Edge 0
* - Instruction = 17
* - Next instruction = 18
* - Conditional next instruction = 18
* - Interrupt = 17
* - Pin = 7
*/
{
/* Program */
0x00025440U,
/* Control */
(0x00024007U | (uint32)((uint32)7U << 8U) | (uint32)((uint32)1U << 4U)),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* ECNT: CCU Edge 1
* - Instruction = 18
* - Next instruction = 19
* - Conditional next instruction = 19
* - Interrupt = 18
* - Pin = 9
*/
{
/* Program */
0x00027440U,
/* Control */
(0x00026007U | (uint32)((uint32)9U << 8U) | (uint32)((uint32)1U << 4U)),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* ECNT: CCU Edge 2
* - Instruction = 19
* - Next instruction = 20
* - Conditional next instruction = 20
* - Interrupt = 19
* - Pin = 14
*/
{
/* Program */
0x00029440U,
/* Control */
(0x00028007U | (uint32)((uint32)14U << 8U) | (uint32)((uint32)1U << 4U)),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* ECNT: CCU Edge 3
* - Instruction = 20
* - Next instruction = 21
* - Conditional next instruction = 21
* - Interrupt = 20
* - Pin = 16
*/
{
/* Program */
0x0002B440U,
/* Control */
(0x0002A007U | (uint32)((uint32)16U << 8U) | (uint32)((uint32)1U << 4U)),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* ECNT: CCU Edge 4
* - Instruction = 21
* - Next instruction = 22
* - Conditional next instruction = 22
* - Interrupt = 21
* - Pin = 17
*/
{
/* Program */
0x0002D440U,
/* Control */
(0x0002C007U | (uint32)((uint32)17U << 8U) | (uint32)((uint32)1U << 4U)),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* ECNT: CCU Edge 5
* - Instruction = 22
* - Next instruction = 23
* - Conditional next instruction = 23
* - Interrupt = 22
* - Pin = 18
*/
{
/* Program */
0x0002F440U,
/* Control */
(0x0002E007U | (uint32)((uint32)18U << 8U) | (uint32)((uint32)1U << 4U)),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* ECNT: CCU Edge 6
* - Instruction = 23
* - Next instruction = 24
* - Conditional next instruction = 24
* - Interrupt = 23
* - Pin = 20
*/
{
/* Program */
0x00031440U,
/* Control */
(0x00030007U | (uint32)((uint32)20U << 8U) | (uint32)((uint32)1U << 4U)),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* ECNT: CCU Edge 7
* - Instruction = 24
* - Next instruction = 25
* - Conditional next instruction = 25
* - Interrupt = 24
* - Pin = 22
*/
{
/* Program */
0x00033440U,
/* Control */
(0x00032007U | (uint32)((uint32)22U << 8U) | (uint32)((uint32)1U << 4U)),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PCNT: Capture Duty 0
* - Instruction = 25
* - Next instruction = 26
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 0
*/
{
/* Program */
0x00034E00U | (uint32)((uint32)1U << 6U) | (uint32)(0U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PCNT: Capture Period 0
* - Instruction = 26
* - Next instruction = 27
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 0 + 1
*/
{
/* Program */
0x00036E80U | (uint32)((uint32)1U << 6U) | (uint32)((0U) + 1U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PCNT: Capture Duty 1
* - Instruction = 27
* - Next instruction = 28
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 2
*/
{
/* Program */
0x00038E00U | (uint32)((uint32)1U << 6U) | (uint32)(2U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PCNT: Capture Period 1
* - Instruction = 28
* - Next instruction = 29
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 2 + 1
*/
{
/* Program */
0x0003AE80U | (uint32)((uint32)1U << 6U) | (uint32)((2U) + 1U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PCNT: Capture Duty 2
* - Instruction = 29
* - Next instruction = 30
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 4
*/
{
/* Program */
0x0003CE00U | (uint32)((uint32)1U << 6U) | (uint32)(4U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PCNT: Capture Period 2
* - Instruction = 30
* - Next instruction = 31
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 4 + 1
*/
{
/* Program */
0x0003EE80U | (uint32)((uint32)1U << 6U) | (uint32)((4U) + 1U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PCNT: Capture Duty 3
* - Instruction = 31
* - Next instruction = 32
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 6
*/
{
/* Program */
0x00040E00U | (uint32)((uint32)1U << 6U) | (uint32)(6U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* Changed by NJ to go to instruction 61 */
/* PCNT: Capture Period 3
* - Instruction = 32
* - Next instruction = 33
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 6 + 1
*/
{
/* Program */ /* Next Instruction (INSTR[61]) */
0x00000E80U | (uint32)((uint32)61U << 13U) | (uint32)((uint32)1U << 6U) | (uint32)((6U) + 1U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PCNT: Capture Duty 4
* - Instruction = 33
* - Next instruction = 34
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 16
*/
{
/* Program */
0x00044E00U | (uint32)((uint32)1U << 6U) | (uint32)(16U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PCNT: Capture Period 4
* - Instruction = 34
* - Next instruction = 35
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 16 + 1
*/
{
/* Program */
0x00046E80U | (uint32)((uint32)1U << 6U) | (uint32)((16U) + 1U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PCNT: Capture Duty 5
* - Instruction = 35
* - Next instruction = 36
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 14
*/
{
/* Program */
0x00048E00U | (uint32)((uint32)1U << 6U) | (uint32)(14U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PCNT: Capture Period 5
* - Instruction = 36
* - Next instruction = 37
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 14 + 1
*/
{
/* Program */
0x0004AE80U | (uint32)((uint32)1U << 6U) | (uint32)((14U) + 1U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PCNT: Capture Duty 6
* - Instruction = 37
* - Next instruction = 38
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 20
*/
{
/* Program */
0x0004CE00U | (uint32)((uint32)1U << 6U) | (uint32)(20U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PCNT: Capture Period 6
* - Instruction = 38
* - Next instruction = 39
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 20 + 1
*/
{
/* Program */
0x0004EE80U | (uint32)((uint32)1U << 6U) | (uint32)((20U) + 1U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PCNT: Capture Duty 7
* - Instruction = 39
* - Next instruction = 40
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 22
*/
{
/* Program */
0x00050E00U | (uint32)((uint32)1U << 6U) | (uint32)(22U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PCNT: Capture Period 7
* - Instruction = 40
* - Next instruction = 57
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 22 + 1
*/
{
/* Program */
0x00072E80U | (uint32)((uint32)1U << 6U) | (uint32)((22U) + 1U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* MOV64: PWM 0 -> Duty Cycle Update
* - Instruction = 41
* - Next instruction = 42
* - Conditional next instruction = 2
* - Interrupt = 1
* - Pin = 31
*/
{
/* Program */
0x00054201U,
/* Control */
(0x00004007U | (uint32)((uint32)1U << 22U) | (uint32)((uint32)31U << 8U) | (uint32)((uint32)2U << 3U)),
/* Data */
12928U,
/* Reserved */
0x00000000U
},
/* MOV64: PWM 0 -> Period Update
* - Instruction = 42
* - Next instruction = 3
* - Conditional next instruction = 41
* - Interrupt = 2
* - Pin = na
*/
{
/* Program */
0x00006202U,
/* Control */
(0x00052007U),
/* Data */
12672U,
/* Reserved */
0x00000000U
},
/* MOV64: PWM 1 -> Duty Cycle Update
* - Instruction = 43
* - Next instruction = 44
* - Conditional next instruction = 4
* - Interrupt = 3
* - Pin = 9
*/
{
/* Program */
0x00058203U,
/* Control */
(0x00008007U | (uint32)((uint32)1U << 22U) | (uint32)((uint32)9U << 8U) | (uint32)((uint32)2U << 3U)),
/* Data */
12928U,
/* Reserved */
0x00000000U
},
/* MOV64: PWM 1 -> Period Update
* - Instruction = 44
* - Next instruction = 5
* - Conditional next instruction = 43
* - Interrupt = 4
* - Pin = na
*/
{
/* Program */
0x0000A204U,
/* Control */
(0x00056007U),
/* Data */
12672U,
/* Reserved */
0x00000000U
},
/* MOV64: PWM 2 -> Duty Cycle Update
* - Instruction = 45
* - Next instruction = 46
* - Conditional next instruction = 6
* - Interrupt = 5
* - Pin = 27
*/
{
/* Program */
0x0005C205U,
/* Control */
(0x0000C007U | (uint32)((uint32)1U << 22U) | (uint32)((uint32)27U << 8U) | (uint32)((uint32)2U << 3U)),
/* Data */
12928U,
/* Reserved */
0x00000000U
},
/* MOV64: PWM 2 -> Period Update
* - Instruction = 46
* - Next instruction = 7
* - Conditional next instruction = 45
* - Interrupt = 6
* - Pin = na
*/
{
/* Program */
0x0000E206U,
/* Control */
(0x0005A007U),
/* Data */
12672U,
/* Reserved */
0x00000000U
},
/* MOV64: PWM 3 -> Duty Cycle Update
* - Instruction = 47
* - Next instruction = 48
* - Conditional next instruction = 8
* - Interrupt = 7
* - Pin = 29
*/
{
/* Program */
0x00060207U,
/* Control */
(0x00010007U | (uint32)((uint32)1U << 22U) | (uint32)((uint32)29U << 8U) | (uint32)((uint32)2U << 3U)),
/* Data */
12928U,
/* Reserved */
0x00000000U
},
/* MOV64: PWM 3 -> Period Update
* - Instruction = 48
* - Next instruction = 9
* - Conditional next instruction = 47
* - Interrupt = 8
* - Pin = na
*/
{
/* Program */
0x00012208U,
/* Control */
(0x0005E007U),
/* Data */
12672U,
/* Reserved */
0x00000000U
},
/* MOV64: PWM 4 -> Duty Cycle Update
* - Instruction = 49
* - Next instruction = 50
* - Conditional next instruction = 10
* - Interrupt = 9
* - Pin = 11
*/
{
/* Program */
0x00064209U,
/* Control */
(0x00014007U | (uint32)((uint32)1U << 22U) | (uint32)((uint32)11U << 8U) | (uint32)((uint32)2U << 3U)),
/* Data */
12928U,
/* Reserved */
0x00000000U
},
/* MOV64: PWM 4 -> Period Update
* - Instruction = 50
* - Next instruction = 11
* - Conditional next instruction = 49
* - Interrupt = 10
* - Pin = na
*/
{
/* Program */
0x0001620AU,
/* Control */
(0x00062007U),
/* Data */
12672U,
/* Reserved */
0x00000000U
},
/* MOV64: PWM 5 -> Duty Cycle Update
* - Instruction = 51
* - Next instruction = 52
* - Conditional next instruction = 12
* - Interrupt = 11
* - Pin = 21
*/
{
/* Program */
0x0006820BU,
/* Control */
(0x00018007U | (uint32)((uint32)0U << 22U) | (uint32)((uint32)21U << 8U) | (uint32)((uint32)0U << 3U)),
/* Data */
0U,
/* Reserved */
0x00000000U
},
/* MOV64: PWM 5 -> Period Update
* - Instruction = 52
* - Next instruction = 13
* - Conditional next instruction = 51
* - Interrupt = 12
* - Pin = na
*/
{
/* Program */
0x0001A20CU,
/* Control */
(0x00066007U),
/* Data */
3199872U,
/* Reserved */
0x00000000U
},
/* MOV64: PWM 6 -> Duty Cycle Update
* - Instruction = 53
* - Next instruction = 54
* - Conditional next instruction = 14
* - Interrupt = 13
* - Pin = 4
*/
{
/* Program */
0x0006C20DU,
/* Control */
(0x0001C007U | (uint32)((uint32)0U << 22U) | (uint32)((uint32)4U << 8U) | (uint32)((uint32)0U << 3U)),
/* Data */
0U,
/* Reserved */
0x00000000U
},
/* MOV64: PWM 6 -> Period Update
* - Instruction = 54
* - Next instruction = 15
* - Conditional next instruction = 53
* - Interrupt = 14
* - Pin = na
*/
{
/* Program */
0x0001E20EU,
/* Control */
(0x0006A007U),
/* Data */
3199872U,
/* Reserved */
0x00000000U
},
/* MOV64: PWM 7 -> Duty Cycle Update
* - Instruction = 55
* - Next instruction = 56
* - Conditional next instruction = 16
* - Interrupt = 15
* - Pin = 31
*/
{
/* Program */
0x0007020FU,
/* Control */
(0x00020007U | (uint32)((uint32)0U << 22U) | (uint32)((uint32)31U << 8U) | (uint32)((uint32)0U << 3U)),
/* Data */
0U,
/* Reserved */
0x00000000U
},
/* MOV64: PWM 7 -> Period Update
* - Instruction = 56
* - Next instruction = 17
* - Conditional next instruction = 55
* - Interrupt = 16
* - Pin = na
*/
{
/* Program */
0x00022210U,
/* Control */
(0x0006E007U),
/* Data */
3199872U,
/* Reserved */
0x00000000U
},
/* WCAP: Capture timestamp
* - Instruction = 57
* - Next instruction = 0
* - Conditional next instruction = 0
* - Interrupt = na
* - Pin = na
* - Reg = T
*/
{
/* Program */
0x00001600U,
/* Control */
(0x00000004U),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/*
* ADD THESE LINES BACK IN WHEN READY TO SWITCH CAP PINS
*/
/* Custom instructions to switch between cap4 pins - Need to have instruction 32 execute this instruction on conditional */
/* BR: Branch
* - Instruction = 58
* - Next Instruction = 33
* - Conditional next instruction = 59
* - Condition = zero flag
* - Interrupt = na
* - Pin = na
* - Continue on to 33 unless condition satisfied
* (which right now is state of zero flag), then jump to 59
*/
{
/* Program */
0x00001A00U | (uint32)((uint32)33U << 13U),
/* Control cond. addr. condition */
(0x00000000U) | (uint32)((uint32)59U << 13U) | (uint32)((uint32)16U << 3U),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PCNT: Capture Duty 4(b)
* - Instruction = 59
* - Next instruction = 60
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 18
*/
{
/* Program */
0x00078E00U | (uint32)((uint32)1U << 6U) | (uint32)(18U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* PCNT: Capture Period 4(b)
* - Instruction = 60
* - Next instruction = 35
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = 18 + 1
*/
{
/* Program */
0x00046E80U | (uint32)((uint32)1U << 6U) | (uint32)((18U) + 1U),
/* Control */
0x00000000U,
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
},
/* ADD: Add value in data field [31:0] to src1 (0x00000000)
* NOTE: all this is really doing is setting result1[31] to one, which sets zero flag,
* which is our branch op (58) conditional
* - Instruction = 61
* - Next instruction = 58
* - Conditional next instruction = na
* - Interrupt = na
* - Pin = na
*/
{
/* Program */
0x00074800U,
/* Control sub-op code src1 (ZEROES) src2 (ONES) dest (instr. data field) */
0x00000000U | (uint32)((uint32)1U << 23U) | (uint32)((uint32)0U << 19U) | (uint32)((uint32)7U << 16U) | (uint32)((uint32)1U << 7U) | (uint32)((uint32)2U << 1U),
/* Data */
0x00000000U,
/* Reserved */
0x00000000U
}
};