Part Number: TMS570LS0432
Recently facing issues while debugging and loading the software to micro controller(TMS5400432BPZQQ1R). The behavior is erratic in nature. I am using XDS110 debug probe.Randomly and gradually I get errors like - (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.3.0.00032)
2.) (Error -2063 @ 0x0)
3.) (Error -2064 @ 0x0)
4.)(Error -1170 @ 0x0)
On reducing the frequency of TCLK still I face the same issue. But the JTAG connectivity test is successful every time I do it.
On replacing the micro controller it works but after few debugging sessions on code composer studio, the error occurs again. Not able to figure out the source of the issue. How to avoid and solve these errors?