This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: EtherCAT Echo Demo

Part Number: TMS320F28379D
Other Parts Discussed in Thread: CONTROLSUITE

I've followed the instructions in SPRUIG9, but when I reach step 8.5 the slave does not reach the "OP" state.

When following the steps to generate the Slave Stack Sources with v5.12, the C28xx was already displayed in the custom selection. However when "OK" is clicked, a SSC Tool configuration file is requested so I pointed at the "C28xx_Config.xml" provided in the SSCToolC28xPatch in the controlSUITE. After clicking "Yes" to proceed with including external files another popup indicated (below) that the patch file cannot be applied. Is the "C28xx_Config.xml" the correct file to select?

Initially the slave wouldn't go past "PRE-OP" until the adjusting the "Stay at PRE-OP until Sync Task started" was unchecked.

Is there any additional steps that I'm missing to make the EchoBack sample work as expected?