Part Number: TMS320F28335
Dear team,
My customer is using eCAN of 28335.
CANTEC=0 CANREC=129 CANES has SA1 error.
After the eCAN of TMS320F28335 is disconnected and reconnected, it cannot sent anymore.
The customer uses the can cycle sending mode of TMS320F28335. A CAN module of the computer is used as the receiving node. There was an SE error at the beginning, what is the reason? How to solve it? When customer switch between the main power supply and the backup power supply, eCAN can no longer communicate.