Other Parts Discussed in Thread: TMS320F2812, SPRC097
Hi Ti guys,
We are two guys using the eZ dsp TMS320F2812 for a University project, and We are using Code Composer Studio v.4.1. And right now we are running a few tests, but facing few troubles regarding the tasks we want the DSP to do for us.
- Give an input to GPIOE0 and constantly see if the pin goes high or low (depending on what input we are giving it (High[1] / Low[0]) by monitoring GPIOA1, with real time silicon refresh.
We are using the example Example_281xIdleWake.c from the TI example files SPRC097 (C281x C/C++ Header Files and Peripheral Examples). The program causes an interrupt to occur when a qudrature (or DC) signal goes from high[1] to low[0].
What we wish to do, is resetting the interrupt register, so we can run the example again a observe the changes we make with real time silicon refresh, without resetting the DSP program, but we don't not know which register we need to reset.
Best regards
Dado and Jonas