Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE
I am getting the below error outputs into my terminal:
<Linking>
warning #10247-D: creating output section "RomWaitStateRegsFile" without a
SECTIONS specification
warning #10247-D: creating output section "SyncSocRegsFile" without a SECTIONS
specification
warning #10247-D: creating output section "Emif1ConfigRegsFile" without a
SECTIONS specification
warning #10247-D: creating output section "Emif2ConfigRegsFile" without a
SECTIONS specification
warning #10247-D: creating output section "XbarRegsFile" without a SECTIONS
specification
warning #10247-D: creating output section "InputXbarRegsFile" without a
SECTIONS specification
warning #10247-D: creating output section "AnalogSubsysRegsFile" without a
SECTIONS specification
warning #10247-D: creating output section "ClbXbarRegsFile" without a SECTIONS
specification
warning #10247-D: creating output section "EPwmXbarRegsFile" without a SECTIONS
specification
warning #10247-D: creating output section "OutputXbarRegsFile" without a
SECTIONS specification
warning #10247-D: creating output section "UppRegsFile" without a SECTIONS
specification
warning #10247-D: creating output section "DevCfgRegsFile" without a SECTIONS
specification
warning #10247-D: creating output section "GpioCtrlRegsFile" without a SECTIONS
specification
In my CPU2 project file. I have included the default nonBIOS and RAM files from the C2000Ware folders for this and have not changed them.
I do not have this issue in my CPU1 project which compiles fine. Why might this error occur?
Thanks,
Joel