Part Number: TMS320F2809
Other Parts Discussed in Thread: SYSBIOS
Hello,
I am trying to setup sysbios on this DSP on custom board but I am unable to get running even the example.
I am using Code Composer Studio Version: 10.3.1.00003


Now that I have the project created it warns me about Cpu freq. When trying to add PLL configuration it does not calculate the frequency (0Hz whatever I input):

So instead I just configure CPU frequency here:

Now I can build and debug but I never get to main. It always hangs here:

I suppose that there is some problem with float config, Could you please point me in the right direction?