Part Number: TMS320F28335
Other Parts Discussed in Thread: C2000WARE
Hello , everyone :
My version of CCS is V10.1.1 ,the chip is TMS320F28335 , PC system is win 10 。
I want to use IQmath ,but i meet some error ,
Q1: if i want to use fixed-point IQ format , should i include IQmath.lib or IQmath_fpu32.lib ? i have set MATH_TYPE = IQMTH in IQmathLib.h file。
Q2: I think IQmath.lib should be added if i want to use fixed-point IQ format ,but i get some warning ," #10204-D could not resolve index library "IQmath.lib" to a compatible library "



I refer C200Ware 3.3 IQmath example , it use IQmath_fpu32.lib。dir is "C:\ti\C2000Ware\C2000Ware_3_03_00_00\libraries\math\IQmath\c28\examples"
who can give some help , thanks very much 。^_^