Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hello guys,
Im reading about Secure boot for C2000 devices (spract3.pdf), but which is written for another processor (2838x), I would need to do code protection and I like the solution with CMAC. Is there an implementation option for 28379d? And there is some example ? In C2000Ware there is none, as it is written in the document (I can not find boot_ex1_cpu1_cpu2_cm_secure_flash_cpu1 ...). Or can another algorithm be used? There is no mention of cmac in the datasheet for 28379d.
Thank you for advice.
- Mark.