This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025C: issue of programming F280025C with C2000 GANG

Part Number: TMS320F280025C
Other Parts Discussed in Thread: UNIFLASH

Hi Expert,

My customer are using C2000 GANGto program F280025C, and it come the issue that fail to program and also seem to lock F280025C unfortunately.

if use uniflash to program the same code, there is no problem,

then if use C2000 GANGto program firstly, it will fail and show "Verification error", try again, then it showed" write to RAM error"

after program with C2000 GANG, device seem locked and it is unable to program the device by CCS and uniflash.

Below are the configuration of  C2000 GANG:

After fail to program F280025 with C2000 GANG which showed " write to RAM error“,try to use uniflash to unlock the device, then also fail as below showed.

Trouble Setting Breakpoint with the Action “Remain Halted ” at 0xc058

for more details, please refer to the error log attached.

Question is:

1, why C2000 GANG fail to program F280025C? they use latest C2000 GANG version.

2. why C2000 GANG be able to lock F280025C?

3. Error log attached showed that it fail when do verification of OTP, does uniflash also have the process of doing the verification of OTP?

c2000- gang烧录28002x芯片问题说明.pdf