Part Number: LAUNCHXL-F28069M
Dear all,
I plugged my F28069M launchpad, into my computer for the first time, it is a brand new launchpad taken out of its anti-static bag. The demo program that runs by default sends the temperature via serial port, which works fine, However, after a couple of minutes of the demo program running, i see that the temperature starts rising quite a bit. And it is hot to the touch. Not so much that you get burned but i definetly can feel the microcontroller is hot. The values received via serial are:
".[u46 Celcius = Ref + 9 .[u45 Celcius = Ref + 8 "
Is this normal? that the microcontroller heats up almost 10 ºC while just running the preprogramed demo software?
It is impossible that it got any form of electrostatic damage, because it is brand new and i took proper precautions... maybe this unit is faulty?
Thank you very much for your time!
Joan Marc