Part Number: TMS320F28379S
Other Parts Discussed in Thread: CONTROLSUITE
Almost same issue as described https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/758274/tms320f280049-cannot-execute-program-after-execution-with-different-entry-point.
When the image is OK:
- Successfully write image into MCU via CCS
- Successfully boots by debugger
- Powered off
- Powered on, then MCU still boots successfully
When the image is NG
- Successfully write image into MCU via CCS
- Successfully boots by debugger
- Powered off
- Powered on, then MCU cannot boot
Here are my codes. Please notice that line GPIO_WritePin(GPIO_PIN_DEBUG_LED0, LOW). When this line is commented out, the image is OK. But, when we keep that line, then the image is NG.
- CCS 10.1.0.00010
- Toolchain: TI v18.1.4.LTS
- ControlSuite: /Applications/ti/controlSuite/device_support/F2837xS/v210/F2837xS_common