Other Parts Discussed in Thread: MOTORWARE
Hi,
I try to use SPIA in a connection with an IMU but have no signal CS when I send message using SPI-Write fonction.
My configuration for the SPI is the following one in hal.c (I used motorware):
For the Pin configuration:
// SPI SDI TO IMU
 GPIO_setMode(obj->gpioHandle,GPIO_Number_16,GPIO_16_Mode_SPISIMOA);
 // SPI SDO TO IMU
 GPIO_setMode(obj->gpioHandle,GPIO_Number_17,GPIO_17_Mode_SPISOMIA);
 // SPI SCLK TO IMU
 GPIO_setMode(obj->gpioHandle,GPIO_Number_56,GPIO_56_Mode_SPICLKA);
 // SPI /SCS TO IMU
 GPIO_setMode(obj->gpioHandle,GPIO_Number_19,GPIO_19_Mode_SPISTEA_NOT);
For the SPI config:
void HAL_setupSpiA(HAL_Handle handle)
{ //Update done by louis S on May 25 2021 to configure SPI A for IMU control
 // the IMU is a LSM6DSM
 HAL_Obj *obj = (HAL_Obj *)handle;
 //Start with a Reset of the SPI
 SPI_reset(obj->spiAHandle);
 SPI_setMode(obj->spiAHandle,SPI_Mode_Master);
 SPI_setCharLength(obj->spiAHandle,SPI_CharLength_16_Bits);
 SPI_setClkPhase(obj->spiAHandle,SPI_ClkPhase_Normal);
 SPI_setClkPolarity(obj->spiAHandle,SPI_ClkPolarity_OutputFallingEdge_InputRisingEdge);
 SPI_setBaudRate(obj->spiAHandle,SPI_BaudRate_1_MBaud);
 SPI_setTriWire(obj->spiAHandle,SPI_TriWire_NormalFourWire);
 SPI_enableTx(obj->spiAHandle);
 SPI_enableTxFifoEnh(obj->spiAHandle);
 SPI_enableTxFifo(obj->spiAHandle);
 SPI_setTxDelay(obj->spiAHandle,0);
 SPI_clearTxFifoInt(obj->spiAHandle);
 SPI_enableChannels(obj->spiAHandle);
 SPI_enableRxFifo(obj->spiAHandle);
 SPI_setSuspend(obj->spiAHandle,SPI_TxSuspend_free);
 SPI_enable(obj->spiAHandle);
 return;
} // end of HAL_setupSpiA() function
And I use the SPI Write function in nthe main loop just to test the signal before connection to the IMU with the following code:
SPI_write(handle->spiAHandle,data_to_send);
 // send dummy message
 SPI_write(handle->spiAHandle,0);
Could you help me to get the CS signal.
Regards
Louis