Other Parts Discussed in Thread: C2000WARE
I wrote a TCP client application on TMDSCNCD28388D board to connect to a server running on PC; the client only receives data from the server and doesn't send any messages, the server message is divided into 2 packets with sizes 1460, and 44 bytes respectively. Even if I enabled reassembly mode in lwipopt.h file, the LWIP stack not assemble the packet, it passes it up to the application layer as it arrives so, instead of passing a single packet after being assembled with size of 1504 bytes its two packets!
Is there any TI LWIP example that tests TCP/IP fragmentation and Reassembly of packets?