Hello,
I'm trying to setup various DMA operations on the 28375D Defino, on core 2. I've found that I cannot get a DMA to complete successfully when it is sourced from Flash (const values defined in FLASHF), or when "const" is applied to a GSx source. Can you confirm these types of sources are not allowed?
Also, I've not had a lot of luck with LSx used as either source or destination of a DMA operation. Should that be allowed?
In all cases above, the DMA register settings are correct, and seem to be processed correctly, but yet the destination results do not end up in the source. If using just GSx, and same exact DMA setup, they do.
Regards,
Robert