Part Number: TMS320F280049C
Hi,
Do GPIO24 and GPIO32 always need to be in the High state when the power is turned on?
For example, GPIO32 can be selected as CAN.
Is it okay to use it as a CAN after booting with Flash?
Or I want to use GPIO24 as the output of the comparator.
The comparator should be a circuit that pulls up high at startup.
Thanks,
Koki