Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hi,
1、According to "TMS3202837xD TRM", there have Debug mode or Test mode. Are they same?
2、When I need to use Debug mode or Test mode, do I need to connect to a external debugger and use CCS?
3、When I receive a message data from mssage object 1, how can I get the result?
1)、Should I get the result from Memory Browser window in CCS with the Message RAM address(0x49030~0x49034)?
2)、Or should I program IF1/IF2 Interface register sets, then get the result from the Register of CAN_IF1DATA / CAN_IF1DATB? Thus, I can get the result from Registers window in CCS?
Thanks!