This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: CPU1 Boots CPU2 at frequency which is different the default 200Mhz

Part Number: TMS320F28388D

Hi,

My project is using F28388D, and CPU1 works at clock 192 Mhz.

So Is possible to boot CPU2 works at 200Mhz? So if not , I want to boot CPU2 to work at the same clock with CPU1 : 192Mzh, What is the value for the macro used in the function "Device_bootCPU2()"?, the default macro is CPU2_BOOT_FREQ_200Mhz     - 0xC800U? I have read the TRM of F28388D, so I can't the information to define the value for macro to boot CPU2 at frequency differrent 200Mhz.

Thanks,